Creating field point objects - Metasys - LIT-12013151 - System Integration - CCURE-Victor Integration - 10.0

NAE Commissioning for C•CURE-victor Integration Application Note

Product
Building Automation Systems > Utilities and Integrations > CCURE-Victor Integration
Document number
LIT-12013151
Version
10.0
Revision date
2018-12-17

About this task

After you create a device object, you can insert a field point that represents a single device Item.

Procedure

  1. In the All Items tree, select the device, then select Insert > Field Point.
  2. On the Destination page, click Next.
  3. On the Selected Definition Mode page, select Manual, select the type of point, then click Next.
    Figure 1. Field Point Object - Type Selection
    ???
  4. In the Vendor Reference field, enter a unique name, then click Next.
    Figure 2. Field Point Object - Data Source
    ???
  5. On the Identifier page, in the upper-right corner of the window, enter a unique identifier, then click Next.
    Figure 3. Field Point Object - Identifier
    ???
  6. On the Configure page, click the Hardware tab.
  7. In the Vendor Configuration Data list, click the ellipses icon to add configuration parameters for the point.
    Figure 4. Field Point Object - Vendor Configuration Data
    ???

    The following table lists the Vendor Configuration Data and their meaning.

    Table 1. NAE Vendor Configuration Data setup of Field Point

    Parameter

    Description

    [1]

    The GUID used to identify the object in C•CURE-victor. The value is configured in C•CURE-victor, and you can obtain it from the C•CURE-victor administrator.

    [2]

    The C•CURE-victor Point ID from the system configuration

    [3]

    The Point ID from the system configuration. For possible values, see C•CURE point mapping tables and victor point mapping tables.

    [4]

    The SubType ID for the points in order to read the values. For possible values, see C•CURE point mapping tables and victor point mapping tables.

  8. Click OK to close the Modify List page, click Next to go to Summary page, then click Finish.