Creating a device object - Metasys - LIT-12013151 - System Integration - CCURE-Victor Integration - 10.0

NAE Commissioning for C•CURE-victor Integration Application Note

Product
Building Automation Systems > Utilities and Integrations > CCURE-Victor Integration
Document type
Application Note
Document number
LIT-12013151
Version
10.0
Revision date
2018-12-17

Procedure

  1. In the All Items Tree, select the C•CURE-victor Integration, then select Insert > Field Device.
    Figure 1. Integration Object - Insert Field Device
    Linux_Isert device
  2. On the Destination page, click Next.
  3. On the Selected Definition Mode page, select Manual, then, in the Vendor Reference field, enter a unique name. Click Next.
    Figure 2. Device Object - Manual
    ???
  4. On the Identifier page, in the upper-right corner of the window, enter a unique identifier, then click Next.
    Figure 3. Device Object - Identifier
    ???
  5. On the Configure page, select the Hardware tab.
  6. In the Vendor Configuration Data list, click the ellipses icon to add configuration parameters for the device.
  7. Click Add to add new parameters and set correct value for each one.
    Figure 4. Device Object - Vendor Configuration Data
    ???

    The following table lists the Vendor Configuration Data and their meaning.

    Table 1. NAE Vendor Configuration Data setup of C•CURE-victor Device

    Parameter

    Description

    [1]

    The GUID used to identify the object in C•CURE-victor. The value is configured in C•CURE-victor, and you can obtain it from the C•CURE-victor administrator.

    [2]

    The Point ID from the system configuration. For possible values, see C•CURE point mapping tables and victor point mapping tables.

    [3]

    The SubType ID for the points in order to read the values. For possible values, see C•CURE point mapping tables and victor point mapping tables.

  8. Click OK to close the Modify List page, click Next to go to Summary page, then click Finish.
  9. On the Extension Wizard page, click Done.