To integrate C•CURE or victor with a Metasys system, complete the following steps:
- Create an Integration object in the NAE, and configure the settings so that the NAE can communicate with the victor web service. For more information, see Creating an integration object.
- Export device and point information from C•CURE or victor and transfer it to the NAE. For more information, see Transferring device and point information.
Note: You can manually add individual C•CURE and victor devices and points in the NAE. For
more information, see Manually adding devices and field points.