Design Considerations - Metasys - LIT-12013151 - System Integration - CCURE-Victor Integration - 10.0

NAE Commissioning for C•CURE-victor Integration Application Note

Product
Building Automation Systems > Utilities and Integrations > CCURE-Victor Integration
Document type
Application Note
Document number
LIT-12013151
Version
10.0
Revision date
2018-12-17

To integrate a Metasys system with a C•CURE or victor system, consider the following points:

  • Ensure that all devices are set up and running properly before attempting to integrate with Metasys networks.
  • Use the License Activator application to check the availability of the web service license for C•CURE and victor. You only require a license for C•CURE or victor if that component is installed. Both C•CURE and victor use the victor web service.
Figure 1. License options for web services