Determining the NAE IP address by using the NCT - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

You can use the Network Engine (NxE) Information and Configuration Tool (NCT) to discover the NAE . To determine the IP address of an NAE by using the NCT to discover the device, start the NCT, click Discover, and look for the NxE in the Discovered Devices list. The NAEs must be connected to the same subnet as the NCT computer for the NCT to detect them. For more information, refer to the NxE Information and Configuration Tool Technical Bulletin (LIT-1201990) .