When an NCE25, NAE35, or NAE45 is powered on, it sends a text string to its serial port that contains helpful information, such as its current IP address and device name. (This functionality is no longer available with the NAE55 at Release 10.0.) This data stream is sent from the RS232C or RS232C A Serial Port. The following table is an example of the data that is sent.
|
Device Information |
Example Output |
|---|---|
|
Host Name |
NAE-1 |
|
DHCP Enabled |
Yes |
|
IP Address |
159.222.8.206 |
|
Subnet Mask |
255.255.252.0 |
|
Default Gateway |
159.222.8.2 |
|
DHCP Server |
159.222.8.9 |
|
MAC Address |
00-80-66-05-0F-FC |
|
Neuron® ID |
00-00-00-00-00-00 |
|
Model Number |
MS-NAE4510-2 |
|
RAM Memory |
122 Mb |
|
NAND Memory |
128 Mb |
|
OS Type |
Linux |
|
COM1 |
115200n8 |
|
Serial/Internal modem |
no |
|
USB Modem |
no |
|
Battery Status |
Good |
To determine the NAE IP address and device name, attach an RS232 DB9 cable between the serial ports of the computer and the NAE, then connect a computer monitor. Install a VT100 terminal emulator program on the computer that connects to the device. Check with your IT department, or technical support team, for a recommended VT100 terminal emulator program to use with your Windows operating system.
- Baud rate=115200
- Data Bits: 8 bit
- Stop Bits: 1
- Control Flow: None