Setting a computer to be compatible with APIPA - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

About this task

If you are configuring an NAE for use on an Ethernet network without DHCP or DNS support, the computer’s IP address must be compatible with APIPA. View the local area connection properties of the active network connection as follows:

Procedure

  1. In Control Panel, select Network and Internet > Network and Sharing Center > Change adapter settings. The Network Connections window appears.
  2. Right-click Local Area Connection and select Properties. The Local Area Connection Properties window appears.
  3. Click Internet Protocol Version 4 (TCP/IPv4) and then click Properties.
  4. Make sure the option Obtain an IP address automatically is selected. This setting allows Windows to provide the network engine with an IP address in the 169.254.x.x range when connected to a network that does not have a DCHP server.