Summary tab - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document type
Commissioning Guide
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

The Summary tab (Figure 1) in the Site Management Portal UI provides a quick view of the status of the objects and items currently in your site.

Select, drag, and drop an object from the Navigation panel in the Display panel, and click the Summary tab. When you first click the Summary tab, the NAE requests the status of the items in the Display panel (Figure 1). This request may take a few minutes.

For additional information and explanations of the attributes found in the Summary and Diagnostic tabs, refer to the Object Help in the Metasys SCT Help (LIT-12011964) or the Metasys Site Management Portal Help (LIT-1201793) .

Figure 1. NAE Summary Tab