Diagnostic tab - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

The Diagnostic tab displays NAE hardware status information that may aid troubleshooting.

With the NAE object selected, click the Diagnostic tab to view current information about the NAE hardware status. Figure 1 shows an example.

Figure 1. NAE Diagnostic Tab

You can also select and drag Network Protocol objects into the Display panel and click the Diagnostic tab to view information for the selected Network protocol (Figure 2).

Figure 2. BACnet Protocol Diagnostic Tab