NAE diagnostic tools - Metasys - LIT-1201519 - MS-NAE35xx-2 - MS-NAE45xx-2 - MS-NAE5510-2U - MS-NAE5510-3U - MS-NAE551S-2 - MS-NAE55xx-3 - MS-NCE25xx-0 - MS-NXE85SW-x - Supervisory Device - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE55 Network Automation Engine - NAE85 Network Automation Engine - NCE25 Network Control Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document type
Commissioning Guide
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

The NAE hardware and UI provide tools for diagnosing and troubleshooting hardware and software problems with the NAE .

The primary NAE diagnostic tools include:

Other tools are also available, such as the SNMP Trap Browser and the ping command for determining the NAE IP address and the ability to communicate on the TCP/IP network. See Determining the NAE IP address and device name for a network connection and Troubleshooting procedures for information on using the Trap Browser and the ping command.