Data protection battery related problems - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

Improper shipping, handling, installing, charging, or disconnecting of the NAE data protection battery may also result in flash memory corruption and data loss.

To avoid problems related to the data protection battery, refer to the Setup and Adjustment sections in the appropriate network engine installation instructions for proper procedures for connecting, charging, and disconnecting the data protection battery before you connect supply power to the NAE. These instructions include:

  • NCE25 Installation Instructions (Part No. 24-10143-63)
  • NAE35/NAE45 Installation Instructions (Part No. 24-10050-6)
  • NAE55/NIE55 Installation Instructions (Part No. 24-10051-43)
  • NIE29 Installation Instructions (Part No. 24-10143-594)
  • NIE39/NIE49 Installation Instructions (Part No. 24-10050-103)
  • NIE59 Installation Instructions (Part No. 24-10143-608)