Corrupted NAE memory - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document type
Commissioning Guide
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

Corruption of nonvolatile NAE flash memory may render an NAE inoperable. Flash memory may become corrupted for a variety of reasons and is one of the most common NAE problems encountered when commissioning, configuring, updating, and operating the NAE.

A typical method to recover from corrupted NAE flash memory includes reloading the NAE disk image and downloading the NAE archive database with a compatible version of the SCT. Refer to the NAE Update Tool Help (LIT-12011524) for information on installing the NAE disk image. Refer to the Metasys SCT Help (LIT-12011964) for information on upgrading NAE archive databases.