Troubleshooting - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document type
Commissioning Guide
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

This section describes the most common problems you may encounter when you set up and operate NAEs . Use the general solution guidelines and procedure references in this section to avoid or resolve these problems. Table 1 provides a list of common NAE problems and their solutions. To troubleshoot the NAE-S, also refer to the NAE-S Commissioning Guide (LIT-12012269) for specific information that applies only to this secure NAE model.

This section is not a troubleshooting guide for Metasys system networks, customer networks, BAS networks, or the field devices connected to the NAE .

Field device troubleshooting is covered in the field device documentation. Refer to the appropriate field device documentation for additional information.

Note: To effectively troubleshoot an NAE , it may be necessary to isolate the NAE from the Ethernet network and the associated field trunks and field devices, and then direct-connect to the NAE with a computer to browse the Site Management Portal UI.