Warning banner - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

As an option, an NAE configured as a Site Director can have a Warning Banner enabled. The Warning Banner is a statement that always appears when operators log on the Site Management Portal of the engine. By default, the network engine is configured not to display a warning banner.

For small-capacity engines, you can select to use the U.S. Department of Defense (DoD) banner. For the large-capacity engines, you have the choice of three different warning banners: U.S. Department of Defense (DoD), U.S. (General Services Administration (GSA)), or U.S. Department of Transportation (DOT) Federal Aviation Administration (FAA). The information in the text window is customized for the United Stated government agency where the Metasys system is installed. The reader must read and accept the conditions in the Warning Banner before logging on. The banner cannot be customized or its text be changed. For steps on how to enable or disable this banner, see Enabling and disabling Warning Banner.

Figure 1. United States DoD Warning Banner