System Configuration Tool (SCT) - Metasys - LIT-1201519 - MS-NAE35xx-2 - MS-NAE45xx-2 - MS-NAE5510-2U - MS-NAE5510-3U - MS-NAE551S-2 - MS-NAE55xx-3 - MS-NCE25xx-0 - MS-NXE85SW-x - Supervisory Device - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE55 Network Automation Engine - NAE85 Network Automation Engine - NCE25 Network Control Engine - 11.0

NAE Commissioning Guide

Brand
Metasys
Product name
NAE35 Network Automation Engine
NAE45 Network Automation Engine
NAE55 Network Automation Engine
NAE85 Network Automation Engine
NCE25 Network Control Engine
Document type
Commissioning Guide
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09
Language
English

SCT is an offline software tool you use to create, edit, save, and restore the various archive and security databases that configure Metasys system networks, OASs, ODSs, ADSs/ADXs, NAEs, NIEs, SNEs, SNCs, and supported field devices. The SCT UI opens in its own window and has a similar appearance to the online Site Management Portal UI (Figure 1). SCT also manages trusted certificates for network engines. For details, see Appendix: Certificate Management.

SCT, if running on a 32-bit Windows operating system, allows commissioning of N2 devices by allowing HVAC PRO software, GX-Tool software, and XTM Configurator software to access the devices on the N2 Bus of an NAE . SCT also allows commissioning of equipment controllers by using the CCT software to access the devices on the field bus of an NAE .

SCT provides a Simulation feature that allows you to simulate an online supervisory device and test a database’s control logic prior to downloading it to an NAE . Using the SCT, you can view and configure multiple sites in one archive.

Figure 1. SCT UI screen example