Reset command device - Metasys - LIT-1201519 - MS-NAE35xx-2 - MS-NAE45xx-2 - MS-NAE5510-2U - MS-NAE5510-3U - MS-NAE551S-2 - MS-NAE55xx-3 - MS-NCE25xx-0 - MS-NXE85SW-x - Supervisory Device - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE55 Network Automation Engine - NAE85 Network Automation Engine - NCE25 Network Control Engine - 11.0

NAE Commissioning Guide

Brand
Metasys
Product name
NAE35 Network Automation Engine
NAE45 Network Automation Engine
NAE55 Network Automation Engine
NAE85 Network Automation Engine
NCE25 Network Control Engine
Document type
Commissioning Guide
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09
Language
English

The Reset Device command in the Site Management Portal UI initiates an orderly reset that saves

recent changes to the SNE archive database and restarts the engine's operating system. When the

SNE requires a reset, the title bar of the object in the Display panel displays Reset Needed. A reset

is required for new settings to take effect after making changes to the following attributes:

• APDU Retries

• APDU Segment Time-Out

• APDU Time-Out

• BACnet IP Port

• Computer Name

• Contact Person

• Domain Name

• Max APDU Length

• Network Address

• Port Number

• Read/Write Community

• SNMP DDA

• SNMP Management Device

• Serial Port 1 Cable Config

• Time Sync Period

Note: Changing the Computer Name value of the SNE forces a device reset.