NAE disk image updates and archive database upgrades - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document type
Commissioning Guide
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

The NAE operating system, Metasys system software, NAE archive database, and recent NAE operation data reside on the NAE disk image.

To update the NAE Metasys system software, use SCT Pro or the NAE Update Tool. Refer to SCT Pro Help (LIT-12013035) and NAE Update Tool Help (LIT-12011524) . For some Metasys releases, the NAE Update Tool is required to update the disk image. If you have a custom integration built by the Johnson Controls Systems Integration Services (SIS) group, you must first back up the protocol DLL and license files with the NIEx9 Driver Manager tool before you update the disk image. If you skip that step, you are not able to restore the DLL and license files to the NAE after you update the engine. Refer to the NIEx9 Driver Manager Application Note (LIT-12011919) . This DLL backup step is not necessary if you are using any of the several pre-configured integrations (Modbus, M-Bus, KNX, C•CURE/victor, Zettler, and OPC UA).

When you update an NAE to a new version of the disk image to the latest release version of the Metasys system software, you must also upgrade the NAE archive database to a new release database. For an overview of the upgrade process, refer to the SCT Installation and Upgrade Instructions (LIT-12012067) .