NAE Object name - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document type
Commissioning Guide
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

The NAE Object Name is an editable attribute on the NAE Focus tab that the Metasys software uses to identify the NAE in the Site Management Portal UI and in the SCT. The Object Name is a label only and may not be the same as the Computer Name. Changing the Object Name merely changes the name that you see in the navigation tree, alarm messages, trend reports, and other screens in the Site Management Portal UI and SCT that refer to the NAE . Changing the Object Name does not impact the object references or network communication with other devices on the site. You can change the Object Name at any time. We recommend an intuitive name that clearly identifies the NAE in the Site Management Portal UI and Metasys site.