Metasys UI - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document type
Commissioning Guide
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

In addition to the Site Management Portal UI, the Metasys Server software installer also installs the Metasys UI software. Metasys UI is a mobile-optimized software component that consolidates existing Metasys user interface products into a single, simplified, and easy-to-learn interface. Metasys UI provides a simple location-based navigation approach to finding information about the Metasys site, including the ability to search for any location or equipment by name and to bookmark a location or equipment in a web browser. All data displayed in the Metasys UI is organized in a dashboard format that gives you the overview of what is happening within a space, equipment, or central plant. You can also and create and manage graphics and their associations to equipment and spaces. Access Metasys UI from any type of client device with any screen size. For more details, refer to the Metasys UI Technical Bulletin (LIT-12012115) .