Metasys Help Files - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

The Metasys Help files provide shared system information and individualized mode-dependent information for the Metasys Site Management Portal (SMP) or the System Configuration Tool (SCT). The Metasys Site Management Portal Help (LIT-1201793) provides information about alarming, commanding, auditing live data values, and other online features. The Metasys SCT Help (LIT-12011964) provides information about offline operations such as managing archives, creating spaces, simulating systems, and establishing equipment and serving relationships.

In either SMP or SCT mode, the Metasys Help menu provides Help files in PDF format. Because last minute changes might occur just before product release, always refer to the Johnson Controls Knowledge Exchange for the most up-to-date version of the Metasys Help files.