MS/TP communications bus - Metasys - LIT-1201519 - MS-NAE35xx-2 - MS-NAE45xx-2 - MS-NAE5510-2U - MS-NAE5510-3U - MS-NAE551S-2 - MS-NAE55xx-3 - MS-NCE25xx-0 - MS-NXE85SW-x - Supervisory Device - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE55 Network Automation Engine - NAE85 Network Automation Engine - NCE25 Network Control Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document type
Commissioning Guide
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

The MS/TP communications bus is a local or remote network that connects supervisory controllers and field controllers to point interfaces using BACnet MS/TP protocol. The remote network, called the Remote Field Bus, requires the addition of a BACnet/IP to BACnet MS/TP Router. The MS/TP bus consists of two types of buses: the FC Bus and the SA Bus. Each bus has its own set of device addresses. For details on how to apply the local and remote MS/TP bus, refer to the FX MS/TP Communications Bus Technical Bulletin (LIT-12011670) MS/TP Communications Bus Technical Bulletin (LIT-12011034) .