Controller Configuration Tool (CCT) - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

CCT is a software tool that you use to configure, simulate, and commission equipment controllers that belong to the Metasys system family, such as CGMs, CVMs, FACs, FECs, IOMs, and VMAs. Among the many helpful CCT options is NxE Passthru, which provides you the means to download an equipment controller over the Metasys network, provided SCT 14.0 and CCT 14.0 are installed on the same computer. For more information on CCT, refer to the Controller Tool Help (LIT-12011147) .