Basic Access operating mode (small-capacity engines only) - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document type
Commissioning Guide
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

Basic Access for small-capacity engines is a mode of operation allowing users with Basic Access user accounts access to a subset of the standard user interface capabilities based on their assigned permissions. Basic Access user accounts are created by Metasys system administrators using the Security Administrator system. Basic Access meets the user interface requirements for most building operators. Basic Access is provided on all of the Metasys system engines and servers but is the primary user interface in the NAE35 controllers.

You cannot commission or configure an NAE35 in Basic Access mode. You must log in to the full Site Management Portal UI on the NAE35 to commission and configure the device. See Login user names and passwords for information on logging in to NAE35 Basic Access.

Note: Network engines upgraded to Release 11.0 no longer offer Basic Access user accounts.