Editing existing alarm parameters - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0
NAE Commissioning Guide
- Product
- Network Engines > Network Automation Engines > NAE55 Network Automation Engine
- Network Engines > Network Automation Engines > NAE35 Network Automation Engine
- Network Engines > Network Automation Engines > NAE45 Network Automation Engine
- Network Engines > Network Automation Engines > NAE85 Network Automation Engine
- Document number
- LIT-1201519
- Version
- 11.0
- Revision date
- 2022-02-09
Procedure
-
In the Site Management Portal UI, select and drag the desired NAE
object or field device object from the Navigation panel and drop
it in the Display panel. The NAE
or field device Focus screen opens.
-
Click the Alarm tab. The Alarm Configuration screen
opens (Figure 1).
Figure 1.
NAE
Alarm Configuration
Tab
-
Select items in the Select Item(s) list to edit existing
alarms. (To create new alarms, see Creating new alarms.)
-
Click Edit and make changes to the desired Attributes
for the NAE
or field device.
-
Click Save to save the edited alarm settings.