Creating new alarms - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document type
Commissioning Guide
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

About this task

You can create new alarms for the NAE or any of the supported field devices on the field trunks attached to the NAE .

Procedure

  1. Select and drag the desired NAE or field device object from the Navigation panel into the Display panel. The NAE or field device object Focus screen opens.
  2. Select the Alarm tab and the device’s Alarm screen opens. Click New and the Insert Alarm Wizard opens (Figure 1).
    Figure 1. Insert Alarm Wizard

  3. Select the device Attribute for which you want to create an alarm.
  4. Follow the Wizard instructions and create or edit the values for the Attribute for which you want to create an alarm.
  5. Click Save when you have finished creating the desired alarm parameters for the device Attribute.