Replacing an NAE - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

About this task

To replace an NAE on a network site, update the site registration to ensure that devices on the site communicate with the new (replacement) engine; otherwise, devices may attempt to communicate with the network engine that was removed from the site.

If you do not remove the NAE from a site correctly, the Site Director may attempt to send messages to the old NAE , creating unnecessary network traffic.

If the NAE's trend data is stored in an ADS repository, forward the data prior to beginning the upgrade by following these steps for each engine:

  1. Select a supervisory engine in the Navigation tree.
  2. Select Action > Commands. A list of available commands appears.
  3. Select Archive, then click Send. The archived trend data is sent to the ADS/ADX.

To replace the NAE:

Procedure

  1. Using the SCT, upload the current copy of the NAE database.
  2. Physically replace the old NAE with the new NAE , connect the new NAE to the network, and power on the new NAE .
  3. Do one of the following:
    • Configure the NAE with the same host name and IP address of the old NAE from the Site Management Portal.
      Note: This configuration lets you download the database with SCT without using the Device Change option.
    • Verify that the SCT can communicate with the NAE , then select the Device Change option when downloading the database with SCT to identify the Site Director and host name of the new NAE .
  4. Download the existing NAE archive database to the new NAE.