Preparing NAE for a network that supports DNS but not DHCP - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

This scenario is not typical of modern networks. The steps are identical to the steps in the Preparing NAE for a network without DHCP and without DNS support when the NAE uses APIPA and Preparing NAE for a network without DHCP and without DNS support when the NAE uses a static IP address.

Using the NAE Ethernet MAC address (from the NAE label), the network administrator can update the DNS server and the assigned computer name. If this is done, you can enter dns-name in Launcher on any computer on the building network.