Entering basic NAE parameters in the focus screen - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

Procedure

  1. In the Site Management Portal UI, display the NAE device object and click the Focus tab.
  2. Click Edit. Edit the NAE Object Name and Description values as required.
    Figure 1. NAE Focus tab (Basic)
  3. Click Save.
  4. Select the Advanced option and click Edit.
    Figure 2. NAE Focus Tab - Advanced Edit Mode
  5. Edit the advanced attribute values as needed. (Refer to the NAE Device Object Help and Audit Trails Help in the Metasys Site Management Portal Help (LIT-1201793) for guidance.)

    If the NAE is on a site with an ADS/ADX, enter the ADS/ADX’s IP address in Local Site Director field in the Site section of this screen. The NAE thereafter reports to the ADS/ADX as its Site Director.