Accessing Site Management Portal UI on an NAE - Metasys - LIT-1201519 - MS-NAE35xx-2 - MS-NAE45xx-2 - MS-NAE5510-2U - MS-NAE5510-3U - MS-NAE551S-2 - MS-NAE55xx-3 - MS-NCE25xx-0 - MS-NXE85SW-x - Supervisory Device - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE55 Network Automation Engine - NAE85 Network Automation Engine - NCE25 Network Control Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document type
Commissioning Guide
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

About this task

After an NAE is set up for connectivity, the Site Management Portal UI can be accessed through the Launcher.

See Site Management Portal user interface and the Metasys Site Management Portal Help (LIT-1201793) for additional information about navigating the Site Management Portal UI.

You need to know the Computer Name (or IP address) of the NAE you wish to access. If you do not know the IP address of the NAE , see Determining the NAE IP address and device name for a network connection.

If the NAE has been added to a building’s DNS server, you can access it by its Computer Name.

To access the Site Management Portal UI on an NAE through the Launcher:

Procedure

  1. Start Launcher.
  2. Select the Computer Name (or IP address) of the NAE on the SMP tab of the Launcher, and click Launch. The Metasys system login window appears.
  3. Type the NAE Username and Password, and then click Login or press Enter.
  4. To view an NAE , select the NAE object from the Navigation panel and drag it to the Display panel. The NAE object opens with the Focus tab active (Figure 1).