Detailed Procedures - Metasys - LIT-1201519 - MS-NAE35xx-2 - MS-NAE45xx-2 - MS-NAE5510-2U - MS-NAE5510-3U - MS-NAE551S-2 - MS-NAE55xx-3 - MS-NCE25xx-0 - MS-NXE85SW-x - Supervisory Device - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE55 Network Automation Engine - NAE85 Network Automation Engine - NCE25 Network Control Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document type
Commissioning Guide
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

You need the following items to perform the detailed commissioning procedures for an NAE :

  • an NAE with Release 9.0.x or 11.0 software

  • an Internet browser on a laptop or desktop computer for downloading the Launcher application that is used to log on the NAE . Supported browsers include Microsoft Edge 44 or later, Google Chrome version 78 or later, or Apple Safari version 11.0 or later

    Note: In some scenarios, the computer must be a DHCP client or must be configured to use a static IP address appropriate for the network.
  • the NAE Ethernet MAC address

  • the NAE Information and Configuration Tool (NCT) installed on the commissioning laptop or computer

You may also need:

  • an Ethernet crossover cable

  • a new, unique IP address for each NAE on the Metasys network if DHCP cannot be used

  • a copy of the NAE archive database that configures the NAE for your specific site. (The NAE archive database can be created and stored offline in the SCT.)

  • SCT Release 14.0 loaded on the commissioning computer