Verifying the Site Director defined for an engine or server - Metasys - LIT-1201519 - MS-NAE35xx-2 - MS-NAE45xx-2 - MS-NAE5510-2U - MS-NAE5510-3U - MS-NAE551S-2 - MS-NAE55xx-3 - MS-NCE25xx-0 - MS-NXE85SW-x - Supervisory Device - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE55 Network Automation Engine - NAE85 Network Automation Engine - NCE25 Network Control Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document type
Commissioning Guide
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

About this task

For time synchronization to work properly, all engines and servers on a site must have the correct name for the Site Director in the Local Site Director attribute. If an engine or server has the wrong Site Director specified, time synchronization on your Metasys site does not work properly. Follow these steps:

Procedure

  1. Log on the engine or server.
  2. Drag and drop the engine or server object to the Display frame.
  3. Select Advanced.
  4. Scroll to the Site section and verify that the Local Site Director attribute contains the correct device (Figure 1). In this example, the Site Director is a network engine (SNE11000-gr1).
    Note: The Local Site Director may be entered as an IP address or host name. If entered as a host name, the name is case-sensitive (for example, SNE11000-gr1 is not the same as sne11000-gr1).
    Figure 1. Site Director Field

  5. If the Site Director field contains the wrong device or is empty, click Edit. Edit the Site Director entry and click Save.