Setting the time zone on the Metasys Server Site Director - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0
NAE Commissioning Guide
- Product
- Network Engines > Network Automation Engines > NAE55 Network Automation Engine
- Network Engines > Network Automation Engines > NAE35 Network Automation Engine
- Network Engines > Network Automation Engines > NAE45 Network Automation Engine
- Network Engines > Network Automation Engines > NAE85 Network Automation Engine
- Document number
- LIT-1201519
- Version
- 11.0
- Revision date
- 2022-02-09
Procedure
-
In the lower-right corner of the Metasys Server computer screen,
click the time. The Date and Time Properties box appears (Figure 1). The appearance of this screen and others vary depending on
the operating system.
Figure 1. Time and Date on a Metasys Server
-
Depending on the operating system, click Change date and time settings
or Date and time
settings. The Date and Time window appears (Figure 2).
Figure 2. Date and Time window on Metasys Server
-
Verify that the Set time automatically option is set to
On.
-
Select the correct time zone under the Time
zone drop-down list box.
-
Select Adjust for daylight saving
time automatically.
-
Close the window to save your changes.