Setting the time zone in the Network Engine Site Director - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

Procedure

  1. Log on the Site Director network engine.
  2. Drag the Site object to the Display frame.
  3. Click Edit.
  4. In the Time section, in the Default Time Zone drop-down box, select the correct time zone for the device (Figure 1).
    Figure 1. Default Time Zone in the Site Object

  5. Click Save.
    Note: The Site object's focus window is updated immediately to indicate the current time and selected time zone, but the blue status bar in the lower right corner does not update until you log off, then log on the network engine again.
  6. Reset the network engine for the time zone change to take effect.