Selecting a site time server for the Metasys Server Site Director (Multicast) - Metasys - LIT-1201519 - MS-NAE35xx-2 - MS-NAE45xx-2 - MS-NAE5510-2U - MS-NAE5510-3U - MS-NAE551S-2 - MS-NAE55xx-3 - MS-NCE25xx-0 - MS-NXE85SW-x - Supervisory Device - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE55 Network Automation Engine - NAE85 Network Automation Engine - NCE25 Network Control Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document type
Commissioning Guide
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

About this task

Follow these steps to select a time server for a Metasys Server Site Director when the time synchronization method is Multicast.

Procedure

  1. Log on the Metasys Server Site Director.
  2. Drag the Site object to the display frame.
  3. Select Advanced.
  4. Click Edit.
  5. In the Time section under the Time Sync Method drop-down box, verify the selection is set to Multicast.
    Figure 1. Time Sync Method field set to Multicast
  6. In the Site Time Servers list, click the browse button and add the IP address or host name of the SNTP Time Server that furnishes the master time to the network engine Site Director. Leave the Device Time Servers list blank.
    Note: Specify a host name only if a DNS server is available to the Site Director.
  7. Click Save.