Restoring default user preferences - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

Procedure

  1. Log on to the SMP user interface of the network engine as the MetasysSysAgent user.
  2. On the Tools menu of the user interface, select Administrator. The Security Administration tool appears.
  3. On the View menu, select User Preference File Names. The user preference file names appear in the Roles and Users pane of the Security Administration tool.
  4. Record the file name of the user whose preferences you want to restore.
    Note: If the user has been removed from the system, there is no record of the user preference file name in the Security Administration tool. In this case, remove user preference files from the network engine that do not have a corresponding user preference file name in the Security Administration tool.
  5. Close the Security Administration tool and continue with Removing user preference files.