Restoring default system preferences - Metasys - LIT-1201519 - MS-NAE35xx-2 - MS-NAE45xx-2 - MS-NAE5510-2U - MS-NAE5510-3U - MS-NAE551S-2 - MS-NAE55xx-3 - MS-NCE25xx-0 - MS-NXE85SW-x - Supervisory Device - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE55 Network Automation Engine - NAE85 Network Automation Engine - NCE25 Network Control Engine - 11.0
NAE Commissioning Guide
- Product
- Network Engines > Network Automation Engines > NAE55 Network Automation Engine
- Network Engines > Network Automation Engines > NAE35 Network Automation Engine
- Network Engines > Network Automation Engines > NAE45 Network Automation Engine
- Network Engines > Network Automation Engines > NAE85 Network Automation Engine
- Document type
- Commissioning Guide
- Document number
- LIT-1201519
- Version
- 11.0
- Revision date
- 2022-02-09
Procedure
-
Using NCT, connect to the network engine on which you want to restore the
default system preferences.
-
Click Start SSH on the
Connections tab. NCT now opens a port to the engine
for you to use.
-
Use an SSH client like PuTTY to log on to the network engine. Use the
MetasysSysAgent credentials.
-
Navigate to the \opt\metasys\var\Preferences directory on
the engine.
-
Delete the file with this command:
rm
SystemPreferences.xml
.
-
Exit from the SSH client and disconnect the engine from NCT.