Copying preferences between devices - Metasys - LIT-1201519 - MS-NAE35xx-2 - MS-NAE45xx-2 - MS-NAE5510-2U - MS-NAE5510-3U - MS-NAE551S-2 - MS-NAE55xx-3 - MS-NCE25xx-0 - MS-NXE85SW-x - Supervisory Device - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE55 Network Automation Engine - NAE85 Network Automation Engine - NCE25 Network Control Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document type
Commissioning Guide
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

Procedure

  1. Using NCT, connect to the source network engine; that is, the one that contains the preferences you want to copy.
  2. Click the Explorer tab, click Refresh Device Contents, then navigate to the Preferences directory for the device as shown in Table 1.
  3. Use Get File in NCT to copy SystemPreferences.xml (system preference) or UserPreferences-userID.xml (user preference), where userID is the identification number that appears in the Security Administration tool.
  4. Paste the file onto the desktop of your computer.
  5. Disconnect the network engine from NCT.
  6. Connect NCT to access the destination network engine (where you want to copy the preferences) as the MetasysSysAgent user and navigate to the Preferences directory for the device as shown in Table 1.
  7. Use the Send File option in the NCT to paste the SystemPreferences.xml file or UserPreferences-userID.xml file that you copied to your computer desktop with Step 4.