Configuring preferences - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

About this task

Note: To configure the preferences of a specific user, you must log in as that user or as a user with Administrator rights.

Procedure

  1. On the Tools menu of the user interface, click Configure Preferences. The Metasys Preferences dialog box appears.
  2. Set the preferences according to the Preferences section of the Metasys Site Management Portal Help (LIT-1201793) .

    If you specified Level 1-4 Sound Files on the Alarm Settings tab, place the alarm sound files into the audio folder on the network engine. Some network engines do not permit the file copy operation because the audio folder is write-protected. The audio folder is located in the following directory:

    For NAE85 :

    C:\Program Files (x86)\JohnsonControls\MetasysIII\UI\audio

    For NCE25/NAE35/NAE45 (Release 9.0.7or later) and NAE55 (Release 10.0):

    NAE Device\opt\metasys\bin\UI\audio\

    Note: If a sound file is missing from the folder, the Metasys system uses the default system beep for that alarm priority.