Configuring and maintaining preferences introduction - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document type
Commissioning Guide
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

The Metasys system provides customized preferences for the user interface. The preferences allow authorized users to configure how the user interface behaves, including the sounds and colors, the startup view, and the ability to add links to external applications that can be accessed from within the user interface of the NAE device.

Some steps in the following sections involve certain file operations, such as copying files and navigating to specific folders. The tool used for these operations is NxE85 the NxE Information and Configuration Tool (NCT) for the NAE . For a hardware engine, log on to the device remotely using the NCT, then use the Get File and Copy File options in the Explorer tab of the NCT.

For information on the NCT, refer to the NxE Information and Configuration Tool Technical Bulletin (LIT-1201990) .