Import certificate - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

Use SCT to import certificates and private keys from the local file system. Three file formats are supported: *.pem, *.cer, and *.crt. Typically, each device has two or three certificate files to import: one root, one intermediate, and one server certificate. Some devices may have more than one intermediate certificate. Whatever the case, always import every certificate file that the customer's IT department or CA provides from the CSR you sent them.

SCT supports the import of only one certificate at a time. For example, if the root and intermediate certificate information comes in a single file, you need to split it into two different files, one for the root and the other for the intermediate certificate.

When you import a server certificate, SCT pairs the imported server certificate with the private key from the associated CSR. If a server certificate is imported that contains an identical Issued To Common Name (CN) as an existing certificate, the imported certificate replaces the existing certificate, but the private key is retained; it is not replaced.