Export certificate - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

Use SCT to export certificates and private keys to the local file system. Exporting certificates is an optional precautionary measure that allows you to export and store certificates to a computer or removable media for safekeeping. Keep in mind that certificates with private keys are sensitive information that you should treat as highly confidential files.

Three file formats are supported: *.pem, *.cer, and *.crt. Typically, each device has two or three certificate files to export: one root, one intermediate, and one server certificate. Some devices may have more than one intermediate certificate. Whatever the case, always export every certificate file that the customer's IT department or CA provides from the CSR you sent them.