Uploading a certificate - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

About this task

To upload a certificate from a network engine to an archive database:

Procedure

  1. Open the archive database.
  2. On the Tools menu, select Certificate Management. The Certificate Management screen appears.
  3. Click the Devices tab. A table of devices with certificates appears. Select the device that has a certificate you want to upload. (If you need to upload the certificates of multiple engines, you can select more than one from the devices table.)
    Figure 1. Uploading a Certificate
  4. Click Upload. The Certificate Upload Wizard appears.
    Figure 2. Certificate Upload Wizard

  5. Specify the username and password of the network engine (or click Communicate via Site Director to use the Site Director's credentials). Click Test Login. When the login is confirmed, click Next to complete the remaining steps in the Certificate Upload Wizard. The ActionQ window appears to indicate the progress of the upload. A completion status of OK indicates that the certificate upload process was successful.
  6. Close the ActionQ window.