Replacing a self-signed certificate - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

About this task

Follow these steps to replace an existing certificate with a new self-signed certificate for a network engine in the archive database. This procedure is useful if you need to replace an expired or compromised trusted certificate with a self-signed certificate.

Procedure

  1. Open the archive database.
  2. On the Tools menu, select Certificate Management. The Certificate Management screen appears.
  3. Click the Devices tab. A table of all devices with certificates appears.
    Figure 1. Devices Tab in Certificate Management
  4. Select the device and click Replace Self-sign.