Backing up a certificate - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

About this task

To back up a certificate for a network engine, create a backup of the archive database using the traditional method in SCT (Tools > Database > Create Backup). In addition to backing up the archive database, this process also backs up the network engine certificates. For details, refer to the Create Backup section in Metasys SCT Help (LIT-12011964). You can also back up and store certificates for safekeeping by exporting each certificate file to a computer or removable media. Refer to the Exporting a Certificate section in Metasys SCT Help (LIT-12011964). Lastly, certificates are also backed up and stored when you export the archive database. Refer to the Export Database section in Metasys SCT Help (LIT-12011964).
Important: As an important restriction for creating and restoring database archive backups that contain network engine certificates, you must use the same SCT computer for both operations. Do not restore the archive using a different SCT computer, or the certificate data is deleted. This is a security precaution that protects against certificate theft.