Certificate list view - Metasys - LIT-1201519 - MS-NAE45xx-2 - MS-NAE55xx-3 - MS-NAE551S-2 - MS-NCE25xx-0 - MS-NAE5510-2U - MS-NAE35xx-2 - MS-NXE85SW-x - MS-NAE5510-3U - Supervisory Device - NCE25 Network Control Engine - NAE55 Network Automation Engine - NAE35 Network Automation Engine - NAE45 Network Automation Engine - NAE85 Network Automation Engine - 11.0

NAE Commissioning Guide

Product
Network Engines > Network Automation Engines > NAE55 Network Automation Engine
Network Engines > Network Automation Engines > NAE35 Network Automation Engine
Network Engines > Network Automation Engines > NAE45 Network Automation Engine
Network Engines > Network Automation Engines > NAE85 Network Automation Engine
Document number
LIT-1201519
Version
11.0
Revision date
2022-02-09

Use the certificate list view to determine if all certificates required by each device reside in the archive. The certificate list view provides these features:

  • Indication of an expired certificate.
  • Indication of whether a certificate is required in one or more certificate chains used by a device in the archive. The list view also makes clear which certificates are not needed and may be deleted.
  • Information about the certificate, including: Issued To, Type, Device Name (server certificates), Expiration Date, Details (for example, SHA1 Thumbprint).
  • Clickable column headers that sort the rows by the data in that column.
  • Options for importing, exporting, and deleting root, intermediate, or server certificates.
Figure 1. Viewing Certificate Details