Workflow - Metasys - LIT-12011829 - Field Device - VMA18 VAV Modular Assembly

N2 VMA Application Note

Product
Variable Air Volume > Modular Assemblies > VMA18 VAV Modular Assembly
Document number
LIT-12011829
Revision date
2018-11-01
Note: At CCT 10.1 and later, you can build N2 VAV Box applications using the VAV Single Duct selection tree in CCT. The VAV Single Duct selection tree builds everything you need for the application, including proper mapping tables. Pre-built applications are no longer included with the installation DVD.
Figure 1. Workflow