Updating the NIE Configuration - Metasys - LIT-12011829 - Field Device - VMA18 VAV Modular Assembly

N2 VMA Application Note

Product
Variable Air Volume > Modular Assemblies > VMA18 VAV Modular Assembly
Document number
LIT-12011829
Revision date
2018-11-01

If the NCM system has been migrated to the Metasys system using NIEs, the NIE may need to rediscover any VMA points in the VMA1832 that are new and delete any VMA14xx points that are no longer used.

Important: If an NIE is using a GIO object to reference a CS object, you must delete and rediscover the GIO object because the CS point attributes have likely changed. Be sure to find and update references to the GIO point attributes.

See the Replacing a VMA14xx with a VMA1832 Controller on an NCM section for more information.