If the NCM system has been migrated to the Metasys system using NIEs, the NIE may need to rediscover any VMA points in the VMA1832 that are new and delete any VMA14xx points that are no longer used.
Important: If an NIE is using a GIO object to reference a CS object, you
must delete and rediscover the GIO object because the CS point attributes have
likely changed. Be sure to find and update references to the GIO point
attributes.
See the Replacing a VMA14xx with a VMA1832 Controller on an NCM section for more information.