References - Metasys - LIT-12011829 - Field Device - VMA18 VAV Modular Assembly

N2 VMA Application Note

Product
Variable Air Volume > Modular Assemblies > VMA18 VAV Modular Assembly
Document number
LIT-12011829
Revision date
2018-11-01
Refer to the following documents for more information:
  • DDL Programmers Manual (LIT-630010)
  • Operator Workstation Technical Bulletin (LIT-636013)
  • Metasys Network Technical Manual Control System Object (LIT-636102)
  • N1 Migration with the NIE Technical Bulletin (LIT-1201535)