Compile the NCM database. If no errors are detected, proceed to GPL Translation.
If errors are detected during the compile process as shown in Figure 1, correct them before proceeding. Errors detected are located in the NC-1.DLT file created by the DDL computer.
Figure 1. Errors Detected during NCM Decompile

Errors are indicated by the caret (^) character and are searchable in the text editor. See Figure 2 for an example NC-1.DLT file with a model name error.
Figure 2. Errors Displayed in NC-1.DLT File

Fix any corresponding error line in the DDL file and recompile the DLT file.